7EN02-0423-03

Acknowledge inhibition (Ack Inhibit.)

You can configure the injection inhibition input to activate the insulation alarm relay when the injection is disabled. This is critical in an UL-FS type environment to obtain a feedback (acknowledgment) on the injection status.

The allowed values for this parameter are ON and OFF. The default value is OFF.

To set the acknowledgement of the inhibition signal ON , select Menu > Settings > I/O Config > Ack Inhibbit > ON.

To set the acknowledgement of the inhibition signal OFF , select Menu > Settings > I/O Config > Ack Inhibbit > OFF.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.