7EN02-0423-03

I/O configuration

You can configure the relay parameters to suit the type of relay output information and configure the injection.

You can access the device I/O parameters by selecting Menu > Settings > I/O Config.

The I/O parameters are:

  • Ins. Al. Relay

  • Prev. Al. Rel

  • Inhibit. Input

  • Ack Inhibit

  • Ack. Al. Relay

  • Corr. Flt. Signal

  • Test w.Relays

  • Inhibition Type

To modify the parameter value, see Parameter modification using the display.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.