7EN02-0423-03

Locating

Applicable for IM400N.

You can use the device with automatic insulation fault locator or manual insulation fault locator to locate the insulation fault.

You can use the IFL12MCN (Twelve-channel insulation fault locator with LCD display (indication for 12 channels with R, C, and Zc display) and one output relay (commercial reference: IMDIFL12MCN)) insulation fault locator.

You can use the XRM manual insulation fault locators. SeeLocating insulating fault manually.

Four values are available for this parameter:

Value Advised Usage
Alarm (Default) The device injects a fault locating current when an insulation alarm is detected and compatible with XD301, XD312, XD308C, and XRM devices.
Prev.Al. The device injects a fault locating current when a preventive insulation alarm is detected and compatible with XD301, XD312, XD308C, and XRM devices.
OFF The device does not inject a fault locating current.
IFL The device injects a fault locating current when an insulation alarm is detected and compatible with IFL12MCN device.

NOTE: Insulation fault location is not compatible with IM400-1700 and P1N voltage/ground adaptors.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.