7EN02-0423-03

Safety precautions

The following safety precautions must be thoroughly implemented before attempting to commission the system, repair electrical equipment or carry out maintenance.

Carefully read and follow the safety precautions described below.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate Personal Protective Equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or other local standards.
  • Turn off all power supplying this device and the equipment in which it is installed before working on or in the equipment.
  • Always use a properly rated voltage sensing device to confirm that all power is off.
Failure to follow these instructions will result in death or serious injury.

NOTICE
Equipment damage
  • Do not open this unit.
  • Do not attempt to repair any components of this product or any of its accessory products.
Failure to follow these instructions can result in equipment damage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.