7EN02-0423-03

Injection

Applicable for IM400THRN.

You can set the level of measurement voltage and measurement current that are injected between the monitored power system and ground.

Four setting are available for this parameter:

Value Measurement current value
20V (Default) < 0.469 mA DC
40V < 0.94 mA DC
60V < 1.56 mA DC
80V < 2.48 mA DC

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.