7EN02-0423-03

Number of Transformer (No. of Transfo)

This parameter is applicable for IM400THRN and when V.Adapt parameter value is set to P1N.

This is the value of number of transformer connected.

Three settings are available for the No. of Transfo parameter:

  • 0

  • 1

  • 3

Example to set Primary DC Resistance and Number of Transformer

If Then
You have connected 3 transformers and DC primary resistance of each transformer is 15 kΩ. Select 15 kΩ value for Pri.DC Resis parameter. Set 3 value for No. of Transfo parameter.
You have connected 1 transformer and DC primary resistance of transformer is 15 kΩ. Select 15 kΩ value for Pri.Dc Resis parameter. Set 1 value for No. of Transfo parameter.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.