7EN02-0423-03

Network configuration

You can configure the electrical network parameters to suit to the electrical applications you want to monitor.

You can access the device network parameters by selecting Menu > Settings > Network.

The network parameters for IM400N are:

  • App

  • Filtering

  • Locating

  • V.Adapt

  • Frequency

  • HRG

The network parameters for IM400THRN are:

  • App

  • Filtering

  • V.Adapt

  • HRG

  • Injection

  • Pre. DC Resis.

  • No. of Transfo.

To modify the parameter value, see Parameter modification using the display.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.