7EN02-0423-03

ON light indicator

If the ON light indicator is red, there is an error in the power system or your device.

The error is one of the following cases:

  • Interruption of the injection circuit

  • Auto test not OK

  • Product error

  • System error

  • Over limit capacitance:

    • C > 500 μF

    • C > 2,000 μF with IM400-1700 voltage adaptor

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.