7EN02-0423-03

Hardware overview

A Display
B Contextual menu buttons
C Menu button to go to the main menu
D Red indicator light for device product status
E Yellow indicator light for Modbus communication indication
F Green indicator light for correct insulation indication
G White indicator light for preventive insulation alarm
H Yellow indicator light for insulation alarm
I Esc button to return to the previous menu or cancel a parameter entry
J Product catalog number
K Serial number
L Auxiliary power supply terminal block
M Injection terminal block
N Insulation alarm relay terminal block
O Preventive insulation alarm relay terminal block
P Modbus communication terminal block
Q Injection inhibition input terminal block

Device commercial reference

Model Commercial reference
IM400N IMDIM400N
IM400THRN IMDIM400THRN
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.