7EN02-0423-03

Mounting and dismounting from a Grid

You can install the device on a grid using fixing brackets (reference 01199 Prisma catalog) or equivalent. The device must not be tilted after installation.When mounting or dismounting the device, you can keep the terminal blocks connected and wired up, or you can remove them. For USA and Canada, the device mounting should be open type only.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.