7EN02-0423-03

Mounting

  1. Position the fixing brackets on the device and tighten the screws and washers as illustrated (tightening torque: 1.2 N.m (8.85 lb-in.).
  2. Attach the device to the grid using clamps.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.