7EN02-0423-03

Flush-mounting and dismounting

You can attach the device to any flat, rigid vertical support using the 3 spring clips supplied. You must not tilt the device after installation. To free up space for control gear, you can attach the device to the front panel of the floor-standing or wall-mounted enclosure. For USA and Canada, the device mounting should be open type only.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.