7EN02-0425-01

Configuring network parameters

  1. Navigate to Menu > Settings > Network.

    The NETWORK screen displays.

  2. Modify the parameters value as per the following table:
    NOTE: Use the contextual menu buttons to modify the parameters value.
    Parameter Allowed Values Default Value Description
    App

    THR

    THR

    THR for medium voltage systems.

    Filtering
    • 2s

    • 20s

    • 200s

    20s

    Select the filtering time depending on the application.
    V.Adapt
    • None

    • P1N

    P1N

    Select the adaptor if the network voltage is greater than the rated network voltage of the device.

    • Select None value for testing the device before installation when P1N is not connected.

    • Select P1N value for during operation when P1N is connected.

    Injection
    • 20V

    • 40V

    • 60V

    • 80V

    60V

    Select the injection depending on the application.

    NOTE: The advised values are 60V or 80V.
    HRG
    • OFF

    • 0.1....2 MΩ

    OFF

    • Select OFF when no grounding resistance is connected.

    • Select the value of the neutral grounding resistance, which is connected to the device.

    Pri.DC Resis

    0....50 kΩ

    0 kΩ

    Select the value of resistance of the compatible Schneider Electric voltage transformer primary winding.
    No. of Transfo
    • 0

    • 1

    • 3

    0

    Select the value of number of transformer connected.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.