7EN72-0185-13

Additional information

Go to www.se.com and search for:

  • your meter’s user manual for configuration and operating instructions.

  • your meter’s installation sheet for installation and basic setup instructions.

  • the ION Reference document for further information about the ION architecture and detailed ION module descriptions.

  • the ION Device Template for information on the configuration of ION modules in your meter’s default template.

Refer to EcoStruxure™ Power Monitoring Expert documents to generate 4-30 reports.

Contact your local sales representative for details on available third-party test lab certifications for your device.

Go to www.iec.ch and search for IEC 61000-4-30 for a complete description of the 4-30 standard.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.