0614IB1702

Masterpact MTZ1 Control Modes

The control mode of the Micrologic X control unit sets how the opening and closing functions of the circuit breaker are controlled.

Two control modes are available: Manual and Auto.

Manual mode only accepts orders made using one of the following:

  • The mechanical buttons on the front of the circuit breaker.

  • The external pushbutton connected to the undervoltage release (MN)/shunt trip (MX)/shunt close (XF).

  • The electrical closing pushbutton (BPFE).

Auto mode has two settings: Local or Remote. All orders accepted in manual mode are accepted in auto mode, as well as orders from local or remote communication as follows:

  • Auto Local: the operator needs to be close to the circuit breaker to establish communication and only orders sent from a local source through communication are accepted:

    • Ecoreach software through the USB connection.

    • Masterpact MTZ Mobile App through Bluetooth with the Masterpact Operation Assistant Digital Module.

  • Auto Remote: the operator does not need to be next to the circuit breaker to establish communication and orders are only accepted sent from a remote source through the communication network.

NOTE: Ecoreach software connected through the communication network can be used to send control orders to the circuit breaker.

The control mode factory setting is Auto Remote.

Masterpact MTZ Operation According to Control Mode Configuration

The following table summarizes the opening and closing operations available, depending on the control mode configured:

Control Mode

Type of Order and Delivery Method

Mechanical

Electrical

Through Communication

Pushbutton

BPFE

Point to point (voltage release)

IO module*

Ecoreach software through USB

Masterpact MTZ Mobile App through Bluetooth + Masterpact Operation Assistant Digital Module

Ethernet Modbus/ TCP

IFE/IEFE Webpages

Manual

—

—

—

—

—

Auto: Local

—

—

Auto: Remote

—

—

Masterpact MTZ Operation in Manual Mode

  1. Micrologic X control unit

  2. ULP port module

  3. Embedded Ethernet interface (EIFE)

  4. Circuit breaker mechanism

  5. Input/output application module (IO)

Opening and closing operations available in Manual mode:

  • 0: mechanical opening pushbutton

  • 1: mechanical closing pushbutton

  • BPFE: electrical closing pushbutton

  • External pushbuttons wired by customer, and connected to:

    • XF: standard or communicating and diagnostic shunt close

    • MX: standard or communicating and diagnostic shunt trip

    • MN: standard or diagnostic undervoltage release

Masterpact MTZ Operation in Auto: Local Mode

  1. Micrologic X control unit

  2. ULP port module

  3. Embedded Ethernet interface (EIFE)

  4. Circuit breaker mechanism

  5. Input/output application module (IO)

Opening and closing operations available in Auto: Local mode:

  • 0: mechanical opening pushbutton

  • 1: mechanical closing pushbutton

  • BPFE: electrical closing pushbutton

  • External pushbuttons wired by customer, and connected to:

    • XF: communicating and diagnostic shunt close

    • MX: communicating and diagnostic shunt trip

    • MN: standard or diagnostic undervoltage release

  • IO: with the Breaker Operation predefined application of the IO module set to local control mode

  • Ecoreach software: command sent through USB connection

  • Masterpact MTZ Mobile App with Masterpact Operation Assistant Digital Module: through Bluetooth low energy wireless communication

Masterpact MTZ Operation in Auto: Remote Mode

  1. Micrologic X control unit

  2. ULP port module

  3. Embedded Ethernet interface (EIFE)

  4. Circuit breaker mechanism

  5. Input/output application module (IO)

Opening and closing operations available in Auto: Remote mode:

  • 0: mechanical opening pushbutton

  • 1: mechanical closing pushbutton

  • BPFE: electrical closing pushbutton

  • External pushbuttons wired by customer, and connected to:

    • XF: communicating and diagnostic shunt close

    • MX: communicating and diagnostic shunt trip

    • MN: standard or diagnostic undervoltage release

  • IO: with the Breaker Operation predefined application of the IO module set to remote control mode

  • Communication: remote command through IFE or EIFE interface

Setting the Micrologic X Control Mode

The Auto or Manual mode can be set as follows:

  • On the Micrologic X display screen, at Home → Configuration → Communication → Control Mode → Mode.

  • With the Masterpact MTZ Mobile App through Bluetooth or USB OTG connection.

The Local or Remote mode can be set as follows:

  • When the IO module is used with the Breaker Operation predefined application, the local or remote mode is defined only by the control mode selector switch wired to the digital input I1 of the IO module.

  • When the IO module is not used with the Breaker Operation predefined application, the local or remote mode can be set as follows:

    • With Ecoreach software through a USB connection.

    • With the Masterpact MTZ Mobile App through Bluetooth or a USB OTG connection.

NOTE:
  • The Local or Remote mode cannot be set on the Micrologic X display screen.

  • When Auto mode is set, the control mode is Auto Local or Auto Remote, depending on the last setting.

Displaying the Micrologic X Control Mode

The control mode (Manual, Auto Local, or Auto Remote) is displayed as follows:

  • On the Micrologic X display screen, at Home → Configuration → Communication → Control Mode → Mode.

  • With Ecoreach software through the USB connection.

  • With the Masterpact MTZ Mobile App through Bluetooth or the USB OTG connection.

  • On the IFE/EIFE webpages.

  • By a remote controller using the communication network.

Micrologic X Control Mode Predefined Events

Changing the control mode settings generates the following events:

Event

History

Severity

Manual mode enabled

Operation

Low

Local mode enabled

Operation

Low

Config. error IO and CU - Local/Remote mode

Configuration

Medium

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.