80459-641-01, Rev. 12

About the Model 6 Motor Control Center

Motor control centers (MCCs) provide the most suitable method for grouping electrical motor control and other related devices in a compact, economical, and free-standing installation. A motor control center is made of standardized vertical sections consisting of totally enclosed, dead front, free-standing structures bolted together. These sections support and house control units, a common bus bar for distributing power to the control units, and a network of wireways and conductor entrance areas to accommodate outgoing load and control wires.

The control units consist of components such as combination motor starters, branch feeder devices, and lighting panelboards. Each is mounted in an individual, isolated compartment having its own cover. When front-of-board unit arrangement is selected, all units are mounted on the front side of the MCC. A 15 in. (381 mm) or 20 in. (508 mm) deep section is provided for front-of-board mounting. The standard MCC width is 20 in. (508 mm) with a 4 in. (102 mm) wide vertical wireway.

An optional 25 in. (635 mm) wide section with a 9 in. (229 mm) wide wireway is also available. Larger sections are available for mounting larger equipment. When a back-to-back arrangement is selected, the units are mounted on both the front and rear of 31 in. (787 mm) or 41 in. (1041 mm) deep structures. There is approximately 1 in. (25 mm) of space between back-to-back sections. The standard height of all MCC structures is 91.5 in. (2324 mm) without the three in. (76.2 mm) lifting angle.

NOTE: Model 6 MCCs may be equipped with top-located pull boxes that can add up to 18 in. of height to the section. MCCs with the ArcBlok 1200 Top Entry options have an 18 in. pull box as standard.

Model 6 MCCs are available with an arc-rated option that provides an arc containment rating tested per ANSI C37.20.7-2007 guidelines. Additional reinforcement and pressure relief features are added to the Model 6 MCC to meet the arc containment rating. Refer to ANSI C37.20.7-2007 for the specific test requirements to which the arc-rated Model 6 MCC has been subjected.

The arc-rated Model 6 MCC can provide enhanced arc containment in case of an arcing fault inside the MCC. This is a valuable feature along with other arc flash enhancements available with Model 6 MCCs. Contact your local Schneider Electric representative for more information on Model 6 MCC arc flash options.

A Model 6 MCC with the arc-rated option includes a label (see Model 6 MCC 100 ms Arc-Rated Option Label and Typical Location on Enclosure) that states the performance and requirements necessary to maintain the rating. The arc containment rating is applicable to the front, sides, and rear of the MCC (defined as Type 2 in ANSI C37.20.7-2007).

This instruction bulletin contains specific instructions on maintaining, modifying, and expanding an arc-rated Model 6 MCC. These instructions must be followed to maintain the arc containment rating of the MCC. To achieve the labeled arc containment rating, the additional 100 Millisecond, Arc-rated MCC, Upstream Over-current Protection Device (OCPD) Requirements must be met.

NOTE: Application of the arc-rated option in Model 6 MCCs meeting the requirements of ANSI C37.20.7-2007 does not eliminate the requirements for use of personal protection equipment (PPE).

Model 6 MCC 100 ms Arc-Rated Option Label and Typical Location on Enclosure


100 Millisecond, Arc-rated MCC, Upstream Over-current Protection Device (OCPD) Requirements

The OCPD external to and upstream of the MCC must meet the following criteria:

  • The current rating of the upstream OCPD must be equal to or less than the main device and main bus rating of the MCC.

  • The voltage rating of the upstream OCPD must be equal to or greater than the voltage rating of the MCC. The maximum voltage is 600 V.

  • The interrupting rating of the upstream OCPD must be equal to or greater than the available short-circuit current. The maximum available short-circuit current is 65,000 A.

  • The instantaneous trip setting (if available) of the upstream OCPD must NOT be turned off and must be set to trip at or below 35,000 A.

  • The short-time delay trip setting (if available) of the upstream OCPD MUST be set to the OFF position; no intentional delay is allowed.

  • Approved circuit breakers that can be used as the upstream OCPD:

    • 15–125 A, PowerPacT™ B-frame circuit breakers manufactured by Schneider Electric

    • 15–150 A, PowerPacT H-frame circuit breakers manufactured by Schneider Electric

    • 175–250 A, PowerPacT J-frame circuit breakers manufactured by Schneider Electric

    • 300–600 A, PowerPacT L-frame circuit breakers equipped with MicroLogic™ trip units, manufactured by Schneider Electric

    • 700–1200 A, PowerPacT PJ- or PL-frame circuit breakers equipped with MicroLogic trip units, manufactured by Schneider Electric

    • 1200–2500 A, PowerPacT R-frame circuit breakers equipped with MicroLogic trip units, manufactured by Schneider Electric

    • 800–1200 A, MasterPacT™ NT and MTZ1 circuit breakers equipped with MicroLogic trip units, manufactured by Schneider Electric

    • 1600–2500 A, MasterPacT NW and MTZ2 circuit breakers equipped with MicroLogic trip units, manufactured by Schneider Electric

  • Approved fuses that can be used as the upstream OCPD:

    • 15–600 A, UL® Listed, Class RK1 from any manufacturer

    • 15–600 A, UL Listed, Class RK5 from any manufacturer

    • 15–600 A, UL Listed, Class J from any manufacturer

    • 700–2500 A, UL Listed, Class L from any manufacturer

Schneider Electric Literature Lists

The following Schneider Electric publications may be useful in the maintenance and regular operation of your Model 6 MCC. Your local Schneider Electric representative can provide them upon your request or you can download these documents at www.schneider-electric.us/en/download.

MCC-related Literature

Title

Publication No.

Schneider Electric Digest

0100CT2401 (EN)

Motor Control Centers (Model 6 Catalog, Class 8998)

8998CT9701 (EN)

Model 6 Arc-Rated Motor Control Centers

80459–654–01 (EN, ES, FR)

Closed Door Racking (CDR) Unit for Square D™ Model 6 Low Voltage Motor Control Centers (LVMCCs)

80459-655-01 (EN, ES, FR)

1600 A Splice Instructions

80459-656-01 (EN, ES, FR)

Location Restrictions for Installing a Three-Inch-High Unit into a Model 6 Motor Control Center (MCC) Instructions

80445-750-01 (EN, ES, FR)

Installing a Pull Box Kit into the Square D Model 6 Arc Rated (AR) Motor Control Center (MCC)

80466-258-01 (EN, ES, FR)

Altistart™ 48 Soft Start Units in Motor Control Centers

80438-069-02 (EN, ES, FR)

Altistart 48 Y-Range Soft Start Controllers Installation Guide

S1A37491 (EN);

S1A37491 (ES);

S1A37491 (FR)

ATS48 User’s Manual

1494409 (EN, ES, FR)

Altistart 48 Soft Starts Maintenance and Repair Guide

30072-451-28 (EN)

Altivar Soft Starter ATS480 User Manual

NNZ85515 (EN);

NNZ85515 (ES);

NNZ85515 (FR)

Altistart 22 Soft Starters in Motor Control Centers

80459-652-01 (EN)

ATS22 User Manual

BBV51330 (EN);

BBV51330 (ES);

BBV51330 (FR)

ATS22–Quick Start Guide

S1A10388 (EN);

S1A10388 (ES);

S1A10388 (FR)

PowerPacT B-Frame 15 to 125 A Circuit Breakers Catalog

0611CT1603 (EN)

PowerPacT B-Frame Circuit Breakers and Automatic Switches–User Guide

DOCA0095EN (EN);

DOCA0095ES (ES);

DOCA0095FR (FR)

LC and LI Circuit Breakers

48040-732-04 (EN, ES, FR)

LA, LAMC, LH, LHMC, SLA and Q4 Circuit Breakers

48049-034-04 (EN, ES, FR)

Motor Circuit Protector (MCP) Settings for PowerPacT H- and J-Frame Motor Circuit Protectors

48940-260-01 (EN, ES, FR)

PowerPacT H- and J-Frame ET Circuit Breakers User Guide

48940-313-01 (EN)

PowerPacT H-, J- and L-Frame Circuit Breaker Catalog

0611CT1001 (EN)

PowerPacT H- and J-Frame Circuit Breaker and Switches–Installation

JYT65471 (EN, ES, FR)

MicroLogic 5 and 6 Electronic Trip Units

48940-312-01 (EN, ES, FR)

PowerPacT H-, J-, and L-Frame Circuit Breakers with MicroLogic™ Trip Units

48940-313-01 (EN, ES, FR)

PowerPacT L-Frame Electronic Trip Circuit Breaker Installation Instructions

JYT65477 (EN, ES, FR)

PowerPacT M-, P-, and R-Frame and NS Circuit Breakers

0612CT0101 (EN)

PowerPacT M-Frame Circuit Breakers

48049-251-01 (EN, ES, FR)

PowerPacT M-Frame Circuit Breaker Data Sheet

0612DB1701 (EN)

PowerPacT P-Frame and NS630b–NS1600 Circuit Breakers

48049-148-05 (EN, ES, FR)

PowerPacT P-Frame Circuit Breaker Data

0612DB1702 (EN)

PowerPacT R-Frame Circuit Breaker Data Sheets

0612DB1703 (EN)

PowerPacT R-Frame and NS1600b-NS3200 Circuit Breakers Installation and User Guide

48049-243-04 (EN, ES, FR)

MasterPacT MTZ MicroLogic X Control Unit User Guide

DOCA0102EN (EN);

DOCA0102ES (ES);

DOCA0102FR (FR)

MasterPacT MTZ1 UL Rated/ANSI Certified 800 to 1600 A Circuit Breakers and Switches

0614IB1702 (EN);

0614IB1702ES (ES);

0614IB1702FR (FR)

MasterPacT MTZ2/MTZ3 UL Rated/ANSI Certified 800 to 6000 A Circuit Breakers and Switches

0614IB1701EN (EN);

0614IB1701ES (ES);

0614IB1701FR (FR)

MasterPacT MTZ2/MTZ3 Drawout Circuit Breaker or Switch-Disconnector Instruction Sheet

NVE35470 (EN, ES, FR)

MasterPacT MTZ1 Drawout Circuit Breaker or Switch

QGH70065 (EN, ES, FR)

MasterPacT MTZ2/MTZ2 Drawout Circuit Breaker or Switch

QGH69563 (EN, ES, FR)

Maintenance and Field Testing Guide for MasterPacT NT and NW Circuit Breakers

0613IB1202 (EN, ES, FR)

MasterPacT NT and NW Universal Power Circuit Breakers

0613CT0001 (EN)

Field Testing and Maintenance Guide for Thermal-Magnetic and MicroLogic Electronic-Trip Circuit Breakers

0600IB1201 (EN);

0600IB1201 (ES);

0600IB1201 (FR)

Energy Reduction Maintenance Setting (ERMS) System Installation and User Guide

NHA67346 (EN, ES, FR)

ULP System for MasterPacT and PowerPacT–User Guide

0602IB1503 (EN);

0602IB1504 (ES);

0602IB1505 (FR)

ULP (Universal Logic Plug) System–User Guide

48940-329-01 (EN, ES, FR)

PowerPacT H-, J-, and L-Frame Circuit Breakers–Modbus Communication Guide

0611IB1302 (EN);

0611IB1303 (ES);

0611IB1304 (FR)

MasterPacT NT/NW and PowerPacT P- and R-Frame–Modbus Communication Guide

0613IB1313 (EN);

0613IB1314 (ES);

0613IB1315 (FR)

IFE Ethernet Interface for LV circuit breaker–Instruction Sheet

HRB49218 (EN, ES, FR)

Modbus Interface Module (IFM)

48940-326-01 (EN)

IO module–Input/Output interface for LV circuit breaker–Instruction sheet

HRB49217 (EN, ES, FR)

TeSys T LTMCU / LTMCUF Control Operator Unit

1639581EN (EN);

1639581ES (ES);

1639581FR (FR)

Enerlin’X EIFE Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker User Guide

DOCA0106EN (EN);

DOCA0106ES (ES);

DOCA0106FR (FR)

Enerlin’X IFE Ethernet Interface for One UL Circuit Breaker User Guide

0602IB1801EN (EN);

0602IB1801ES (ES);

0602IB1801FR (FR)

MotorLogic Plus Network Communication Module, Class 9999 Type MB11 and Type MB22 Programming Guide

30072-013-102 (EN, ES, FR)

AC Magnetic Contactors and Starters, Size 00

30072-013-52 (EN, ES, FR)

AC Magnetic Contactors and Starters, Size 0

30072-013-22 (EN, ES, FR)

AC Magnetic Contactors and Starters, Size 1

30072-013-23 (EN, ES, FR)

AC Magnetic Contactors and Starters, Size 2

30072-013-24 (EN, ES, FR)

AC Magnetic Contactors and Starters, Size 3

30072-013-25 (EN, ES, FR)

AC Magnetic Contactors and Starters, Size 4

30072-013-26 (EN, ES, FR)

AC Magnetic Contactors and Starters, Size 5

30072-013-47 (EN, ES, FR)

AC Magnetic Contactors and Starters, Size 6

30072-013-60 (EN, ES, FR)

Full Voltage Contactors and Starters

8502CT9701 (EN)

Reduced Voltage Starters Type S

8600CT9601 (EN)

MotorLogic™ Solid-State Overload Relay

30072-013-29 (EN, ES, FR)

TeSysTM T LTM R EtherNet/IP with a Third-Party PLC–Quick Start Guide

DOCA0119EN (EN);

DOCA0119EN (ES);

DOCA0119EN (FR)

TeSys T LTMR Motor Management Controller User Guide

DOCA0127EN (EN);

DOCA0127ES (ES);

DOCA0127FR (FR)

TeSys T LTMR Motor Management Controller Installation Guide

DOCA0128EN (EN);

DOCA0128ES (ES);

DOCA0128FR (FR)

TeSys T LTMR Motor Management Controller Modbus Communication Guide

DOCA0130EN (EN);

DOCA0130ES (ES);

DOCA0130FR (FR)

TeSys T LTMR Motor Management Controller PROFIBUS DP Communication Guide

DOCA0131EN (EN);

DOCA0131ES (ES);

DOCA0131FR (FR)

TeSys T LTMR Motor Management Controller CANopen Communication Guide

DOCA0132EN (EN);

DOCA0132ES (ES);

DOCA0132FR (FR)

TeSys T LTMR Motor Management Controller DeviceNet Communication Guide

DOCA0133EN (EN);

DOCA0133ES (ES);

DOCA0133FR (FR)

TeSys Tera Motor Management Controller–LTMTCU Control Operator Unit User Guide

DOCA0233EN (EN)

TeSys Tera Motor Management Controller–User Guide

DOCA0257EN (EN)

TeSys Tera Motor Management Controller Installation Guide

DOCA0356EN (EN)

TeSys Tera Motor Management Controller–Modbus RTU Communication Guide

DOCA0355EN (EN)

TeSys Tera Motor Management Controller–PROFIBUS DP Guide

DOCA0256EN

TeSys Tera Motor Management Controller–Ethernet Communication Guide

DOCA0258EN

TeSys Tera Motor Management Controller–Substitution Guide

DOCA0278EN

Harmony™ 9001K/SK/KX 30 mm Push Buttons

9001CT1103 (EN)

Harmony XB4 Metal pushbuttons, switches and pilot lights

DIA5ED2121212EN (EN);

DIA5ED2121212FR (FR)

Harmony XB5 Plastic pushbuttons, switches and pilot lights

DIA5ED2121213EN (EN);

DIA5ED2121213FR (FR)

Harmony™ XB7 Monolithic 22 mm Push Buttons

DIA5ED2120503EN (EN);

DIA5ED2120503EN (ES);

DIA5ED2120503FR (FR)

PowerLogic Circuit Monitor Series 2000 Reference Manual

3020IM9806 (EN)

Altivar Process Variable Speed Drives ATV930, ATV950 Installation Manual

NHA80932 (EN);

NHA80935 (ES);

NHA80933 (FR)

Altivar Process Variable Speed Drives ATV930, ATV950, ATV960, ATV980 Programming Manual

NHA80757 (EN);

NHA80760 (ES);

NHA80758 (FR)

Altivar Process Variable Speed Drives ATV630, ATV650 Installation Manual

EAV64301 (EN);

EAV64307 (ES);

EAV64302 (FR)

Altivar Process Variable Speed Drives ATV630, ATV650, ATV660 Programming Manual

EAV64318 (EN);

EAV64322 (ES);

EAV64320 (FR)

PowerLogic PM5500 Series User Manual

HRB1684301 (EN);

HRB1684303 (ES);

HRB1684302 (FR)

PowerLogic PM8000 Series User Manual

7EN02-0336 (EN);

7ES02-0336 (ES);

7FR02-0336 (FR)

PowerLogic ION9000 Series Installation Guide

NVE78642 (EN, ES, FR)

PowerLogic ION9000 Series User Manual

7EN02-0390 (EN);

7ES02-0390 (ES);

7FR02-0390 (FR)

PowerLogic RD192 Display Installation Guide

QGH42230 (EN, ES, FR)

Altivar Machine ATV320 Variable Speed Drives for Asynchronous and Synchronous Motors Installation Manual

NVE41289 (EN);

NVE41292 (ES);

NVE41290 (FR)

Altivar Machine ATV320 Variable Speed Drives for Asynchronous and Synchronous Motors Programming Manual

NVE41295 (EN);

NVE41298 (ES);

NVE41296 (FR)

ATV320 Modbus® Manual

NVE41308 (EN)

ATV320 CANopen Manual–VW3A3608, VW3A618, VW3A628

NVE41309 (EN)

ATV320 PROFIBUS® DP Manual–VW3A3607

NVE41310 (EN)

ATV320 PROFINET® Manual–VW3A3627

NVE41311 (EN)

ATV320 Modbus TCP-EtherNet IP Manual: VW3A3616

NVE41313 (EN)

ATV320 DeviceNet Manual: VW3A3609

NVE41314 (EN)

MasterPacT MTZ Unpacking Instruction Sheet

PHA53377 (EN, ES, FR)

Thermal Monitoring Dongle Kit Instruction Bulletin

MFR21149 (EN, ES, FR)

Square D Wiring Diagrams for Contactors, Starters, Relays, and Controllers

0140CT9201 (EN)

MasterPacT MTZ–Modbus Communication Guide

DOCA0105EN (EN);

DOCA0105ES (ES);

DOCA0105FR (FR)

iMCC-related Literature

Title

Publication No.

LTM CU–Instruction Sheet

AAV6665701 (EN, ES, FR)

ATS48 Modbus Manual

1623736 (EN, ES, FR)

TeSys T LTM R Modbus Motor Management Controller User’s Manual

DOCA0130EN (EN);

DOCA0130ES (ES);

DOCA0130FR (FR)

TeSys T LTMR PROFIBUS Motor Management Controller User's Manual

DOCA0131EN (EN);

DOCA0131ES (ES);

DOCA0131FR (FR)

TeSys T LTMR CANopen Motor Management Controller User's Manual

DOCA0132EN (EN);

DOCA0132ES (ES);

DOCA0132FR (FR)

TeSys T LTM R DeviceNet™ Motor Management Controller User’s Manual

DOCA0133EN (EN);

DOCA0133ES (ES);

DOCA0133FR (FR)

TeSys T LTMR Motor Management Controller Ethernet Communication Guide

DOCA0129EN (EN);

DOCA0129ES (ES);

DOCA0129FR (FR)

TeSys T LTMR Motor Management Controller Modbus Communication Guide

DOCA0130EN (EN);

DOCA0130ES (ES);

DOCA0130FR (FR)

TeSys T LTM R PROFIBUS-DP® Motor Management Controller Quick Start Guide

1639573US (EN);

1639573 (ES);

1639573 (FR)

TeSys T LTM R CANopen Motor Management Controller Quick Start Guide

1639574 (EN);

1639574ES (ES);

1639574FR (FR)

TeSys T LTM R DeviceNet Motor Management Controller Quick Start Guide

1639575EN (EN);

1639575ES (ES);

1639575FR (FR)

TeSys T LTM R Modbus/TCP Motor Management Controller Quick Start Guide

1639576EN (EN);

1639576ES (ES);

1639576FR (FR)

TeSys T LTM CU Control Operator Unit User’s Manual

1639581EN (EN);

1639581 (ES);

1639581 (FR)

LTM R–Instruction Sheet

AAV7709901 (EN, ES, FR)

LTM E–Instruction Sheet

AAV7950501 (EN, ES, FR)

PowerTag System–Design and Commissioning Guide

DOCA0194EN (EN);

DOCA0194FR (FR)

Altivar Process Variable Speed Drives ATV630, ATV650, ATV660 Programming Manual

EAV64318 (EN)

Altivar Process ATV600 Variable Speed Drives for Asynchronous and Synchronous Motors Embedded Ethernet Manual

EAV64327 (EN)

Altivar Process ATV600 Variable Speed Drives for Asynchronous and Synchronous Motors EthernetIP Modbus TCP Manual–VW3A3720

EAV64328 (EN)

Altivar Process 600 PROFIBUS DP Manual–VW3A3607

EAV64329 (EN)

Altivar Process 600 Variable Speed Drives for Asynchronous and Synchronous Motors DeviceNet Manual–VW3A3609

EAV64330 (EN)

Altivar Process ATV600 Variable Speed Drive for Asynchronous and Synchronous Motors CANopen Manual–VW3A3608, 618, 628

EAV64333 (EN)

Altivar Process Variable Speed Drives ATV930, ATV950, ATV960, ATV980 Programming Manual

NHA80757 (EN);

NHA80760 (ES);

NHA80758 (FR)

Altivar Process 900 Ethernet Manual–Embedded

NHA80940 (EN)

Altivar Process 900 PROFIBUS DP Manual–VW3A3607

NHA80941 (EN)

Altivar Process 900 Variable Speed Drives for Asynchronous and Synchronous Motors DeviceNet Manual–VW3A3609

NHA80942 (EN)

Altivar Process 900 CANopen Manual–VW3A3608, 618, 628

NHA80945 (EN)

Altivar Process 900 Variable Speed Drives EtherCAT Manual–VW3A3601

NHA80946 (EN)

ATS480 Embedded Modbus Manual

NNZ85539 (EN)

ATS480 Ethernet IP Modbus TCP Manual–VW3A3720

NNZ85540 (EN)

ATS480 Profibus DP Manual–VW3A3607

NNZ85542 (EN)

ATS480 CANopen Manual–VW3A3608, VW3A3618, VW3A3628

NNZ85543 (EN)

ATS480 Communication Parameter Addresses

NNZ85544 (EN)

TeSys Tera Motor Management Controller–LTMTCU Control Operator Unit User Guide

DOCA0228EN

TeSys Tera Motor Management Controller–User Guide

DOCA0253EN

TeSys Tera Motor Management Controller Installation Guide

DOCA0254EN

TeSys Tera Motor Management Controller–Modbus RTU Communication Guide

DOCA0255EN

TeSys Tera Motor Management Controller–PROFIBUS DP Guide

DOCA0256EN

TeSys Tera Motor Management Controller–Ethernet Communication Guide

DOCA0258EN

TeSys Tera Motor Management Controller–Substitution Guide

DOCA0278EN

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.