Lock OFF / ON Provisions for Heavy Duty Safety Switches
Lock off provisions are standard on Heavy Duty Safety Switches.
Lock-on provisions are also available as a factory modification on
Type 12 and 304 Stainless Steel Type 4X enclosures.
Lock OFF / Lock ON Options for Heavy Duty Switches
Lock Off Guard Kits
For field installed kits, the lock off guard works by covering the lockout tagout openings whenever the switch is in the ON POSITION. This protects against a padlock from being inadvertently inserted into the switch lockplate. Available ONLY for use on Type 1, Type 3R, Type 12, Heavy Duty Safety Switches.
Lock On
Obtain by using the Safety Switches Product Selector on www.se.com/us.