Square D Load Center SPDs
Square D™ QO, NQ, and Homeline Load Center SPDs are easy to install plug-in units that install as quickly as a standard
circuit breaker. The surge suppressors use two pole spaces in a QO
or Homeline load center, or NQ panelboard. Additional information
can be found on the QO2175SB and HOM2175SB product ranges.
QO, NQ, and Homeline Load Center SPDs
US and Canadian UL Listed as Type 1 SPD to the UL 1449 standard. Complies with requirements of NEC Article 285 (2017), CSA C233.1-87, and CSA C22.2 No. 8-M1986 as appropriate. Meets NEC2023 Section 215, 225 and 230 requirements.
-
QO2175SB for QO load centers, combination devices, and NQ panelboards
-
HOM2175SB for Homeline load centers and combination devices
-
Requires two pole spaces
-
LED indicates operational status
-
Whole House Protection: 25 kA surge current capacity per phase
-
UL Nominal Discharge Current rating of 10 kA