Whole Home Surge Protection — Overview
Residential SPDs
Square D™ Whole Home Surge Protection blocks the voltage spikes at the load center, providing downstream protection for connected devices. These SPDs meet National Electrical Code® section 230, 215 and 225 code requirements.
Whole Home Surge Protective Devices
QO2175SB |
HOM2175SB |
HEPD25 |
QO250PSPD |
HOM250PSPD |
HEPD50 |
HEPD80 |
|
|---|---|---|---|---|---|---|---|
![]() |
![]() |
![]() |
![]() |
![]() |
![]() |
![]() |
|
|
Surge Current |
25 kA |
50 kA |
80 kA |
||||
|
UL Nominal |
10 kA |
20 kA |
10 kA |
20 kA |
|||
|
NEMA Enclosure Rating |
Install in panel |
NEMA 4X |
Install in panel |
NEMA 4X |
|||
|
Approximate
Dimensions |
3.7 x 1.5 x 2.6 |
3.7 x 2.0 x 2.6 |
2.7 x 3.7 x 2.1 |
4 x 1.5 x 2.6 |
4.0 x 2.0 x 2.6 |
3.2 x 3.7 x 2.1 |
|
|
Load Center |
QO |
Homeline |
Any brand load center |
QO |
Homeline |
Any brand load center |
|
|
Installation |
Wiring required |
Plug-on Neutral No wiring required |
Wiring required |
||||
|
Status |
LED |
LED |
LED |
LED |
LED |
LED |
LED |
|
Optional Accessories |
— |
— |
Flush Mounting Kit HEPD25MKF |
— |
— |
Flush Mounting Kit HEPD58MKF |
|
|
Pages |
HEPD SPDs | ||||||