QOB Bolt-on Circuit Breakers
QOB Bolt-on Circuit Breakers with Visi-Trip™ for NQ Panelboards
QOB bolt-on circuit breakers feature a durable bolt-on mounting system. These breakers ensure secure, vibration-resistant installation and consistent electrical performance. The integrated Visi-Trip™ indicator offers a clear visual signal when the breaker has tripped, allowing for quick identification of faulted circuits and faster troubleshooting. QOB bolt-on circuit breakers are designed for use in Square D™ NQ panelboards and are available in a range of amperages and interrupting ratings. These breakers are built for quick installation and long service life.
note
For additional information, refer to NO Panelboards online.