Control Transformers — Overview

Square D™ Industrial Control Power Transformers set the industry standard for design innovation and performance. They are designed with low impedance windings for voltage regulation, and can accommodate the high inrush current associated with contactors, starters, solenoids, and relays. A variety of designs are available to meet the diverse needs of panel builders and machinery OEMs. For complete information including application examples, wiring diagrams, and accessory options, refer to document number 9070CT9901.

Industrial Control Transformers (Types T and TF)

Type T (9070T) transformers are designed with low impedance windings for excellent voltage regulation and can accommodate the high inrush current associated with contactors, starters, solenoids, and relays. Type T transformers are manufactured using the most advanced insulating materials and are the best choice if size and cost are of concern.

Type TF (9070TF) transformers include factory-installed primary and secondary fuse blocks. Type TF transformers consist of two primary fuse blocks and one secondary fuse block. The primary includes rejection-style clips to increase the AIC ratings for the fuses. Since the fuse blocks are mounted on the top of the transformer, Type TF transformers are interchangeable with Type T transformers except for their increased height.

Refer to the following for additional information, selection, and wiring diagrams.


Selection Guide

  1. Determine the inrush and sealed VA of each coil in the control circuit and the VA of all other components.

  2. Total the sealed VA of all operating coils and the VA of all other loads. (This determines the minimum VA size required for the circuit.)

  3. Total the inrush VA of all coils that are starting at the same time and all loads and coils that are running.

  4. Locate a value in the VA column of the Regulation Chart for Type T table shown below, that is equal to or greater than the value calculated in step 2.

  5. In the VA row selected in step 4, find the inrush value under the appropriate voltage regulation column. If this value is greater than the calculated value from step 3, this is the correct transformer VA rating.

    If the inrush value on the selected VA row is not greater than the calculated value from step 3, use the next higher transformer VA rating, that is, the rating on the next row.

If your supply voltage is stable and fluctuates less than 5%, Schneider Electric recommends you use the 90% secondary voltage column. If your supply voltage is not stable and fluctuates more than 10% we recommend you use the 95% secondary voltage column. We recommend that you never use the 85% secondary voltage column since magnetic devices lose life expectancy if they are continuously started at 85% of rated voltage.

Regulation Chart for Type T

VA

Inrush VA @ 20% power factor

Inrush VA @ 40% power factor

95%
Secondary
Voltage

90%
Secondary
Voltage

85%
Secondary
Voltage

95%
Secondary
Voltage

90%
Secondary
Voltage

85%
Secondary
Voltage

50

  193

266

339

151

215

282

75

  271

396

20

210

318

430

100

  339

499

659

266

404

549

150

  666

893

1120

529

731

942

200

  588

815

1041

459

659

866

250

 1416

1910

2388

1057

1494

1936

300

 1634

2184

2709

1194

1681

2169

350

 1894

2592

3261

1392

2005

621

500

 3197

4104

4981

2374

3195

4019

750

 3770

5515

7231

2887

4391

5945

1000

 6587

9079

11430

4706

6886

9051

1500

19324

23983

28607

15066

19361

23756

2000

31384

38777

6161

24794

31630

38667

3000

26539

39934

52713

19355

30721

42216

5000

53111

85265

116277

39368

66309

93882

Feedback