DUG_Iconic Connected Switch 10AX_PDL-00

Example of an automation

This demonstration shows you how to create an automation to switch on the light at the scheduled time.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > Schedule.
    • Tap Repeat (A), select the days you want to set the schedule and tap Save.

    • Set the time (B) at which the automation must start and tap Next.

  4. Tap Add task > Run the device > Iconic Switch.
  5. Tap Switch > On (C) and tap Save.

  6. Tap Next.
  7. In the Automation Settings page, tap Save.
    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable/disable it.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.