DUG_Iconic Connected Switch 10AX_PDL-00

LED indicator mode

Using the Wiser app, you can select the LED indicator mode for easy identification of the device status.
To set the LED indicator modes:
  1. On the Home page, tap All devices > Iconic Switch.
  2. On the device control panel page, tap Settings.
  3. Tap LED indicator Mode (A) and select any one of the following:
    • Reverse With Load: LED on the switch is on when the device is off.
    • Consistent With Load: LED on the switch is on when the device is on.
    • Always Off: LED on the switch is always off.
    • Always On: LED on the switch is always on.

    For information on LED color during each modes, refer to LED Indication.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.