DUG_Iconic Connected Switch 10AX_PDL-00

Removing the device

Using the Wiser app, you can remove a device from the device list.
  1. On the Home page, tap All devices > Iconic Switch.
  2. Tap to display more details.
  3. Tap Remove and Factory Reset Device (A).
    TIP: On the Home page, tap and hold the Iconic Switch to remove the device.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to resetting the device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.