DOCA0236EN-00

About the Book

Document Scope

This document provides the steps required in EcoStruxure™ Control Expert Classic software to create a project with a TeSys™ island and a logic/motion controller using the Modbus TCP protocol.

This document also provides the details about:

  • Integrating the TeSys island into the EcoStruxure Control Expert Classic project.

  • Accessing the TeSys island DTM (Device Type Manager) via EcoStruxure Control Expert Classic software for configuring the TeSys island modules and processes by using TeSys avatars.

  • Using the function blocks of the TeSys island library that is available in EcoStruxure Control Expert Classic software for developing applications and to control TeSys avatar modules.

It is recommended that before using this document, the user must have knowledge on:

  • Information on functionality, structure, and configuration of the TeSys island

  • Information on functionality, structure, and configuration of the controller

Validity Note

This guide is only valid for:

  • EcoStruxure Control Expert Classic software v15.0 SP1 – Classic

  • PLC Modicon M580

Online Information

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download/.

The technical characteristics of the devices described in the present document also appear online. To access the information online, go to the Schneider Electric home page.

Related Documents

Title of documentation

Reference number

TeSys island – System Guide

8536IB1901EN

TeSys island DTM Library Online Help

Available with the installer

Modicon M580 – Hardware Reference Manual

EIO0000001578

EcoStruxure Control Expert – TeSys island Library Control User Guide

EIO0000004519

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.