DOCA0236EN-00

Configuring the IP Address of the TeSys island

Perform the below steps to configure the IP address of the TeSys island:

Step

Action

1

Double-click the CPU in the DTM Browser window.

Result: The device configuration window is displayed on the screen.

2

Select TeSys island device > Address Setting menu, and configure the IP address of the TeSys island.

3

Click Apply.

4

Click the Build icon () on the toolbar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.