DOCA0236EN-00

Uploading TeSys island Project to PLC

Perform the below steps to upload the TeSys island project to PLC:

Step

Action

1

Establish the connection between the PC and PLC by performing one of the following steps:

  • Connect to the PLC by using the IP address.

  • Connect the USB ground cable (BMXXCAUSBH018) between the PC and the front panel of the PLC M580.

2

Click the Connect icon () on the toolbar.

3

Click the Download icon () on the toolbar.

Result: The Transfer Project to PLC window is displayed on the screen.

4

Click Transfer.

Result: The TeSys island project is uploaded to the PLC.

5

Double-click the CPU in the DTM Browser window.

Result: The communication window is displayed on the screen.

6

Select Channel Properties > IP Address Source (PC), and click OK.

7

Right-click on the CPU name in the DTM Browser window and select Connect.

8

Right-click on the TeSys island device in the DTM Browser window and select Connect.

9

Based on the specific requirement, you can choose one of the following steps to configure the TeSys island:

  • If the TeSys island has already been configured and the user does not want to upload a new configuration, right-click on the TeSys island device in the DTM Browser window and select Load data from device.

  • If the TeSys island has not been configured and the user wants to upload a new configuration, perform one of the following steps as required:

    • Double-click on the TeSys island device in the DTM Browser window and configure the device.

    • Right-click on the TeSys island device in the DTM Browser window, and click Device menu > Additional functions > Import > Import TeSys island Configurator Format to import the configuration files.

      Result: The new configuration is imported into the software.

10

Double-click the TeSys island device in the DTM Browser window, and select Store data to device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.