DOCA0236EN-00

Using Function Blocks for Developing Application

Perform the below steps to use the function block for developing the application in EcoStruxure Control Expert Classic software:

Step

Action

1

In Project Browser window, click Programs >Tasks > MAST > Logic.

2

Right-click on the Logic folder and select New Section.

Result: The New Section window is displayed on the screen.

3

Enter a new name to the function block. Select language FBD and click OK.

Result: The configuration zone window is displayed on the screen.

4

Right-click on the configuration zone and select FFB Input Assistant.

Result: Function Input Assistant window is displayed on the screen.

5

Click the Browse button located next to Function Input Assistant screen.

Result: FFB Type Selection window is displayed on the screen.

6

On FFB Type Selection screen, select <Libset V15.0> > TeSys island Library 2021 and then select the required function block and click OK.

7

After selecting the function block, click OK on the Function Input Assistant screen.

Result: An icon appears near the arrow of the mouse.

8

Left-click on the configuration zone.

Result: The structural view of the function block is displayed on the screen.

For more information on the available functional blocks and its configuration, refer to the EcoStruxure Control Expert – TeSys island Library Control – User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.