DOCA0236EN-00

Configuring Project Settings

Perform the below steps to configure the project settings:

Step

Action

1

Open the generated .stu or .xref file in EcoStruxure Control Expert Classic software.

2

Click Tools > Project Settings.

Result: Project Settings window is displayed on the screen.

3

Click Variables and select the Allow dynamic arrays (ANY_ARRAY_XXX) check box to avoid the detected error E1208 usage of dynamic arrays is disabled reported when compiling the project.

4

Clear the Force references initialization check box.

5

Click Languages > Common and select the Allow multi assignment [a=b=c] {ST/LD} check box to avoid the detected error E1203 usage of multi assignment statements is disabled reported when compiling the project.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.