DOCA0161EN-02

Degree of protection - IP•• (IEC 60529)

Defines device protection against the penetration of solid objects and liquids, using two digits specified in IEC 60529 standard. Each digit corresponds to a level of protection, where 0 indicates no protection.

  • First digit (0 to 6): Protection against penetration of solid foreign objects. 1 corresponds to protection against objects with a diameter less than 50 mm, 6 corresponds to total protection against dust.

  • Second digit (0 to 8): Protection against penetration of liquids (water). 1 corresponds to protection against falling drops of water (condensation), 8 corresponds to continuous immersion.

The enclosure of TeSys Power - Giga motor circuit breakers provides a minimum of IP40 (protection against objects less than 1 mm).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.