DOCA0161EN-02

Thermal image of the rotor and stator

The thermal image models the thermal behavior of a motor rotor and stator, taking into account temperature rise caused by overloads or successive starts, and the cooling constants. For each motor power rating, the algorithm takes into account a theoretical amount of iron and copper which modifies the cooling constants.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.