DOCA0161EN-02

Ui: Rated insulation voltage

The rated insulation voltage of an equipment is the value of voltage to which dielectric tests and creepage distances are referred. In no case shall the maximum value of the rated operational voltage exceed that of the rated insulation voltage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.