DOCA0161EN-02

TeSys GV5 / GV6 Devices

Description

TeSys GV5 / GV6 devices offer current ratings from 150 to 500 A, for AC power systems up to 690 Vac.

TeSys GV5 / GV6 devices are available in the following frame sizes:

  • TeSys GV5 for current ratings from 150 to 220 A

  • TeSys GV6 for current ratings from 320 to 500 A

TeSys GV5 / GV6 devices have the following features:

  • Direct rotary handle

  • 3-pole devices

  • 5, 10 and 20 trip classes

  • The following accessories are optional and installable on site:

    • Voltage trip releases

    • Auxiliary contacts

    • Insulation accessories

Device Identification

The commercial reference of each device provides information about:

  • The size of the device

  • The type of protection the device provides

  • The current rating of the device

  • The breaking capacity of the device

For example, the commercial reference of the GV5P 220H device contains the following information:

  • GV5: The device is a TeSys GV5 device.

  • P: The device offers protection against overloads and short-circuits.

  • 220: The device has a current rating of 220 A.

  • H: The breaking capacity of the device is 70 kA at 415 Vac.

Breaking Capacity

The following table shows the breaking capacity (Ics = Icu) in kA rms for TeSys GV5 / GV6 devices:

AC power systems

TeSys GV5P 150F

TeSys GV5P 150H

TeSys GV5P 220F

TeSys GV5P 220H

TeSys GV6P 320F

TeSys GV6P 320H

TeSys GV6P 500F

TeSys GV6P 500H

230 Vac

85 kA

100 kA

85 kA

100 kA

40 kA

100 kA

40 kA

100 kA

400/415 Vac

36 kA

70 kA

36 kA

70 kA

36 kA

70 kA

36 kA

70 kA

440 Vac

35 kA

65 kA

35 kA

65 kA

30 kA

65 kA

30 kA

65 kA

500 Vac

30 kA

50 kA

30 kA

50 kA

25 kA

50 kA

25 kA

50 kA

660/690 Vac

8 kA

10 kA

8 kA

10 kA

10 kA

10 kA

10 kA

10 kA

Standard Compliance

TeSys GV5 / GV6 devices are compliant with the following standards:

  • IEC/EN 60947-2 and IEC/EN 60947-4-1 for motor protection circuit breakers

  • UL 60947-4-1 for motor protection circuit breakers

  • CSA-C22.2 No.60947-4-1 for motor protection circuit breakers

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.