DOCA0161EN-02

About the Book

Document Scope

This guide provides users, installers, and maintenance personnel with technical information needed to operate TeSys Power - Giga Motor Protection Frame 5 and Frame 6 devices in compliance with the IEC/EN and UL/CSA standards:

  • In IEC/EN standards, TeSys Power - Giga Frame 5 and Frame 6 devices are motor circuit breakers.

  • In UL/CSA standards, TeSys Power - Giga Frame 5 and Frame 6 devices are manual motor protectors.

In this guide:

  • The term device covers:

    • Motor circuit breakers

    • Manual motor protectors

  • TeSys Power - Giga Motor Protection Frame 5 devices are referred to as TeSys GV5 devices in this guide.

  • TeSys Power - Giga Motor Protection Frame 6 devices are referred to as TeSys GV6 devices in this guide.

Validity Note

This document applies to TeSys GV5 and TeSys GV6 devices.

Online Information

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download.

The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric home page at www.se.com.

Related Documents

Title of documentation Reference number

TeSys Motor Control and Protection Components Catalog

MKTED210011EN

TeSys GV5P - Motor Circuit Breaker (IEC) and Manual Motor Protector (UL/CSA) - Instruction Sheet

MFR49208

TeSys GV6P - Motor Circuit Breaker (IEC) and Manual Motor Protector (UL/CSA) - Instruction Sheet

MFR49209

You can download these technical publications and other technical information from our website at www.se.com/ww/en/download.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.