DUG_Wiser_Airzone_WH-05

Creating an automation

The following is an example of creating an automation to start the Airzone devices in different modes during a specific instance.
To create an automation:
  1. On the Home screen, tap > Automation > .
  2. Tap and choose an icon that best represents your automation.
  3. Enter a name of the automation (A) and select any of the following conditions to meet (B).
    • All conditions: All conditions must be met to trigger an automation.
    • Any condition: Any one of the condition must be met to trigger an automation.
  4. Tap Add conditions (C) and select any of the following (D):
    • Device status change (Select the device)
    • Away Mode (Enable or Disable)
    NOTE: Maximum 10 conditions can be added.

  5. Select a device (E) that will set the condition.
    IMPORTANT: If you have selected the condition as Away Mode and action as Control a Device then this automation will override your Away Mode settings.
  6. Select the options you want to configure:
    1. Tap (F) and drag the sliding bar up/down (G) to adjust the temperature as per need and tap Set.
    2. Tap (H) and select a mode (Heating or Cooling) of your choice and tap Set.
    NOTE: To remove an added condition, swipe left and tap . Then add a new condition with the required parameters.
  7. To set a specific time for your automation, tap When > Add time and select any of the following (I):
    • Specific time of the day: Sunrise, Sunset, Custom.
    • Period of time: Daytime, Night time, Custom.
    NOTE:
    • Max. 10 entries can be added

    • To remove a specific time, swipe left and tap .

  8. To add an action, tap Then > Add an action and select any of the following (J):
    • Control a device: Select a device that you want to trigger.
    • Send notification: Turn on the notification for the automation.
    • Activate a moment: Select the moment that you want to trigger.
    • Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.

    NOTE:
    • Maximum 10 actions can be added.

  9. For example, tap Control a device > Climate and select any of the following (K):
    • Boost
    • Setpoint
    • Mode
    • On / Off
    1. Tap Boost to set the duration for heating or cooling mode (L).
    2. Tap Setpoint to set the desired temperature (M).
    3. Tap Mode to set the desired mode (N).
    4. Tap On /Off to set the state (P).
  10. Again, tap Add an action and select Wait option.
  11. Scroll through the minutes and set the wait time to 1 minute. Then, tap Set located on the upper right corner.
  12. Tap Save.
    The saved Automation is displayed on theAutomationpage. Tap thetoggle switch (Q) to enable/disable the Automation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.