DUG_Mureva EVlink_Socket_WH-06

Configuring EV Socket LED

You can change the status of the socket LED as per your need to easily identify the on / off and charging functions.
  1. On the Control tab, tap All > Mureva EVlink Socket > Device settings.
  2. On the Device Details page, tap Socket LED and select any one of the following (A):
    • Default:
      • Pulsing green LED during charging

      • Solid green LED in ON state, but not charging.

      • LED is off when socket is in OFF state.

    • Switch OFF after 10 seconds: LED will indicate same as Default behavior but will switch off after 10 seconds. Any change in status will re-trigger the LED.
    The settings will be saved automatically.

    For changing the LED settings without Wiser App, refer to LED settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.