DUG_Mureva EVlink_Socket_WH-06

LED indications

Pairing the device

User Action

LED Indication

Status

Press the push button 3 times

LED blinks amber, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a time, before turning Off.

Resetting the device

User Action

LED Indication

Status

Press the push button 3 times and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and LED is off after reset.

Setting (Default state)

LED behavior

LED color

Status

User action

LED is OFF

Device is OFF.

Out of the box state.

Short press to turn off the Device.

Blinking Orange Device is trying to join a Hub. Short press 3 times when device is not connected during security time-out.
Solid Orange (5 seconds) Device is not part of Hub and security time-out passed. Short press 3 times when security time-out passed.
Blinking Green Device is already connected to Hub. Short press 3 times when device is connected to Hub.
Device is freshly powered ON. Device is switched ON first.
Changing LED behavior from default When the output is OFF, press and hold the push-button for 15 seconds, the LED behavior changes from default to switch off state after 10 seconds. Repeat the same step to return to the default mode. Refer to Configuring Socket LED.
Solid Green Device is ON, power consumption is less than < 10 W.

Turn the device ON via push-button or Wiser Home app.

Pulsing Green Device is ON, power consumption is more than 10 Watts. The car started charging so the power consumption is high.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.