DUG_Mureva EVlink_Socket_WH-06

Resetting the device

You can reset the EV Socket to factory default. It can be reset manually at any time, e.g. when the Hub is replaced.
IMPORTANT: The factory reset can be performed only within 5 minutes of power cycle. After 5 minutes, you cannot do factory reset with push-button.

Short press the push button 3 times and then hold for 10 seconds to reset the device to the factory default mode.
The LED blinks red after 10 s, and then release the push button.

NOTE: All configuration data, user data and network data are deleted.

After factory reset, LED will be off.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.