Pairing the device with Wiser Hub
- On the Home screen, tap
.
- Tap > Appliances > .
- Tap Scan QR code and allow the Wiser
Home app to access your camera. Then, scan the QR code located on
the device.IMPORTANT:
-
The QR code is located on the back side of the device and is not visible when it is mounted on the wall. Refer to the installation instructions for removal and reinstallation of the device.
-
If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.
If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:
-
(A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid.
-
(B): Tap this option if you are unable to find the Mac Address/EUI–64 and Install code.
-
- Tap Next, short press the push button 3 times and make sure that the LED blinks amber.
- Once the device is joined, tap
(A) and select an icon suitable for your load and tap Save.
NOTE: Electric plug icon is assigned by default. - Tap
(B) to enter the name of the device.
- Tap Next and assign the socket to
a new room or an existing room and tap Submit.IMPORTANT: The next screen shows the Device Settings page, where you have the option to configure the settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit. For more information on device settings, refer to Configuring the device section.