Pairing the device with the Wiser Hub
- On the Home screen, tap
.
- Tap > > Flush Mount Thermostat.
- Select your flush mount thermostat from the list.
- Tap Scan QR code and allow the Wiser
Home app to access your camera. Then, scan the QR code located on
the device.IMPORTANT:
-
The QR code is located on the device and is not visible when it is mounted on the wall. It may be located back of the insert or on the side of the insert. Refer to the following installation instructions for removal and reinstallation of the device:
-
Connected Thermostat Insert 2 A (S520619, S530619, S540619)
-
Connected Thermostat Insert 2 A (S920502, S940502)
-
- If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 5.
If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:
-
(A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI-64 and Install code are valid.
-
(B): Tap this option if you are unable to find the Mac Address/EUI-64 and Install code.
-
- Tap Next.
- On thermostat, press and hold + and – touch button simultaneously (> 3 s) until Jn appears on
the display.The wireless
LED blinks amber when joining.
Wait for a few seconds until the wireless
LED on the thermostat turns green and the app confirms that the device has joined.
NOTE: The wirelessLED on the thermostat turns red if it is unable to connect. For more information, refer to Troubleshooting.
- Enter a thermostat name, and then tap Next.
- Assign a thermostat to the room and then tap Submit.NOTE: If the thermostat's preset is set to P3 (Hydronic Underfloor) and it is connected to a Wiser Underfloor Heating (UFH) actuator, then assign a room and tap Next to configure UFH. Refer configuring UFH actuator to completed the setup.
After you pair the device, a success screen appears with the following options:
-
+ Add New Device: Tap to continue pairing more devices.
-
Start Using Your Device: Tap to start using the paired device.
NOTE: The success screen appears only if you are logged in as a Home Owner.The thermostat is now listed on the Control tab under the All and the specific room tabs.
-