DUG_Odace - Thermostat 2 A_WH-08

Resetting the device

You can manually reset the thermostat to factory settings or soft reset.

Soft reset

  1. Press and hold + and touch button simultaneously for > 20 s.


    The thermostat displays “Sr”, indicating soft reset, and it is selected when the button is released.
    The ‘Sr’ will flash to confirm the soft rest.
    NOTE: In case you keep pressing touch button for 25 s then the thermostat will reset to the factory default.
    NOTE: To cancel the soft reset keep press and hold + and touch button simultaneously for > 30 s. This reverts the thermostat's UI back to its previous state before the touch button is pressed, with no change in a functional state.

    A soft reset will:

    • Delete all Zigbee connection details.

    • Revert to the default setpoint in manual control.

    • Maintain all Factory settings e.g. MAC address.

    • Maintain the installer configuration of the device to ensure proper functioning until and after rejoining/re-registration.

Factory reset

  1. Press and hold + and touch button simultaneously for > 25 s.


    The thermostat displays “Fr”, indicating factory reset, and it is selected when the button is released.
    The ‘Fr’ will flash to confirm the factory reset.

    NOTE: To cancel the factory reset keep pressing + and touch button simultaneously for > 30 s. This reverts the thermostat's UI back to its previous state before the touch button is pressed, with no change in a functional state.
    NOTE: When the touch button is released, the "Fr" flashes on the matrix display, and the thermostat resets to factory defaults and after 5 s it returns to preset.

    Resetting to the factory state will:

    • Delete all Zigbee connection details.

    • Delete all configuration data.

    • Revert to the default setpoint in manual control.

    • Maintain all Factory settings e.g. MAC address.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.