DUG_Odace - Thermostat 2 A_WH-08

Creating a Moment

A Moment allows you to group multiple actions that are usually done together. Using the Wiser app, you can create moments based on your needs (such as movie night).

To create a moment:

  1. On the Home page, tap .

  2. Go to Moments > + to create a moment.
  3. On the Moment creator page, enter the Moment name (for example, Movie night).

    TIP: You can choose the cover image that represents your Moment by tapping .

  4. Tap Add actions and select the device that you want to include in a Moment.

  5. Tap Done > Save.

    NOTE: Maximum of 60 actions can be added in a moment.
  6. Tap Save.

    TIP: You can view saved moment on the Home page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.