DUG_Odace - Thermostat 2 A_WH-08

Setting the room temperature using the app

Using the Wiser Home app, you can adjust the room temperature for heating and cooling.

Heating

  1. On the Control tab, tap All devices or a room tab where the thermostat is located.

  2. Tap to select the thermostat.

  3. Adjust the room temperature using the slider control for heating:

    Thermostat functions:

    • : Room temperature is below the set point, so the heating is turned on.

    • : Room temperature is above the set point, so the heating is turned off.

    TIP: You can also adjust the set-point temperature:
    • By tapping or in the heating section on the Control tab.

    • By adding the thermostat to your Favourites. To know more about Favourites, refer to the Managing Favorites topic in the respective System User Guide.

    TIP: Tapping you can set the boost time and later it turns off when the boost time ends.

    IMPORTANT:
    • When the boost time is set, the system automatically increases the set-point temperature by 2 °C for the duration of the boost. Once the boost period ends, the temperature returns to the last set-point.

    • Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.

Cooling

  1. On the Control tab, tap All devices or a room tab where the thermostat is located.

  2. To select a thermostat, tap .

  3. Use the slider control and set the room temperature for cooling.

    NOTE:
    • The indicates that the room temperature is higher than the desired temperature (set point), so the cooling is on.

    • The indicates that the room temperature is lower than desired temperature (set point), so the cooling is off.

    TIP: You can also adjust the set-point temperature:
    • By tapping or of the cooling section on the Control tab.

    • When you add it to your Favourites. To know more about Favourites, refer to the Managing Favorites topic in the respective System User Guide.

    TIP: You can initiate boost on & off anytime tapping .
    IMPORTANT: Once the boost time is set, the set-point temperature automatically decreases by 2° C for the set boost time. After the boost time is over, the set-point temperature returns to the current scheduled event or to the previous set-point temperature.
NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.