DUG_Ovalis Shutter_WH-08

Troubleshooting

Symptom

Solution

Connected shutter cannot be controlled.

  • Check power supply.

  • Remove power to the blind control switch and then re-connect power again.

  • Check the load.

  • In the case of an external push button, check the wiring.

  • Re-couple devices.

Shutter is not driving to the desired position.

Reset to factory default settings, refer to Resetting the device

Shutter is not moving in set time.

Calibrate again.

TIP: See also LED Indications – Understanding LED status and corresponding corrective actions.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.