DUG_PTC_WH-06

Using the device

The Control Panel allows you to switch the device On and Off and control various settings.

On the Control tab, tap ALL device or a room tab where the Plug is located, an icon to open Device Control Screen.

On the Device Control Screen, you can see the following:

A

Switch to turn on/off the device.

B

Current state of the device.

C

Create or assign a schedule

D

Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to in the respective System User Guide

E

Device settings to change the configuration.

NOTE: If you only have single PowerTag in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.