DUG_SysM - Connected Thermostat 2 A, ZB_WH-08

About the device

The SysM - Connected Thermostat, ZB (hereinafter referred to as thermostat) is mainly used for water-based heating and cooling applications, such as water-based underfloor heating and radiator heating.

The thermostat consists of:

  1. Connected Thermostat Insert 2 A (MEG5777-0000)

  2. Frame

  3. Connected Thermostat Module, ZB (MEG5779-0xxx)

NOTE: The thermostat insert 2 A is not suitable for directly connecting an electrical heating.

The thermostat is composed of three components: inserts, frame, and ZB module, and each must be ordered separately.


Thermostat features:

  • Measure & control the room temperature

  • Dot-matrix displays (current room and set temperature)

  • Device lock

  • Valve Protection

  • Heat/cool changeover

  • Universal input setback/presence (external)

  • Volt-free or live control, normally open or normally closed.

  • Smart schedule through a Wiser app

Operating elements

  1. Dot-matrix display

    • Wireless connectivity LED ()

    • Heat and cool demand LED ()

    TIP: All LED indications are explained in the LED behavior chapter.
  2. Rotary push-button

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.