Advanced device settings
To do advanced settings:
Valve Protection
Activate output every two weeks to prevent valve calcification.
Cooling Control
Before enabling Cooling Control mode, identify your system configuration and follow the below scenarios:
Scenario 1
If the heat pump is connected directly to the Underfloor Heating (UFH) device:
-
Enable Cooling Input on the UFH device (Device Details > Cooling Input). Refer to Enabling Cooling Input.
-
Disable Cooling Control mode on all thermostats.
Scenario 2
If the heat pump is connected directly to the thermostat (CFMT) device:
-
Enable Cooling Control on the connected thermostat (Advanced Settings > Cooling Control).
-
Disable Cooling Input mode on the UFH device.
-
Disable Cooling Control mode on all other thermostats.
Scenario 3
If a third-party UFH system is used and the CFMT thermostat acts as a relay:
-
Enable Cooling Control on the thermostat connected to the heat pump (Advanced Settings > Cooling Control).
-
Disable Cooling Control mode on all other thermostats.
Output Relay
This option is to turn off the relay, if used as a temperature measurement device.
Relay Cycle Time
In advanced settings, you
can choose relay cycle time. This setting determines the length of
each on/off cycle of the output relay. The percentage of time within
that cycle time that the relay is on is varied based on demand. A
longer cycle time may be more appropriate for slow heating surfaces,
such as a concrete floor. A short cycle time is more appropriate for
faster heating surfaces, such as an electric panel heater.
For example, 20 mins = three cycle per hour.
Tap Relay Cycle Time (C) and choose any (D):
-
5 mins
-
10 mins
-
20 mins
-
30 mins
Universal Input
Universal Input can provide
a setback of 2° C when input is controlled by a setback timer
or a room proximity sensor. In advanced settings, you can choose Universal
Input.
Tap Universal Input (E) and choose any (F):
-
Disabled – Any change of state on the input is ignored on room occupancies.
-
Presence Detect – Input presence indicates that the room is occupied.
-
Setback – Indicates thermostat should follow unoccupied setpoint.
When the universal input is configured
for presence detection and detects room occupancy, the thermostat
adheres to the user-set setpoint. Upon detecting the room as unoccupied,
the thermostat maintains the same setpoint for the next occupancy
time which is set in room settings. If there is no change in occupancy
status during this period, the thermostat reverts to the unoccupied
setpoint.
Refer room settings for more information on occupancy
duration.
When presence detect or setback has been activated, thermostat dot matrix display shows away mode as below indicating input detection.
Example for heating mode: If the user sets the thermostat's setpoint to 23° C Celsius and the inputs detect room occupancy, the thermostat will adhere to the 23° C setpoint. However, if the room becomes unoccupied, the thermostat will maintain the 23° C setting for the next 10 mins before transitioning to the unoccupied setpoint of 21° C, which is 2° C lower than the user's initial setting.
Example for cooling mode: If the user sets the thermostat's setpoint to 18° C Celsius and the inputs detect room occupancy, the thermostat will adhere to the 18° C setpoint. However, if the room becomes unoccupied, the thermostat will maintain the 18° C setting for the next 10 mins before transitioning to the unoccupied setpoint of 20° C, which is 2° C higher than the user's initial setting.