DUG_SysM - Connected Thermostat 2 A, ZB_WH-08

Changing the device location

Using the Wiser Home app, you can change the thermostat location.
To change the thermostat location:
  1. On the Home page, tap .
  2. Tap Devices > > Location (A) for any of the following:
    TIP: You can also select a device from the list in the Control tab, tap > Device Settings.
    • To create a new room, enter the room name (B) and tap Submit.

    • Change the device location (C).

    NOTE: To remove the device from the room, tap Remove from Room(D).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.