DUG_SysM - Connected Thermostat 2 A, ZB_WH-08

Locking user interface

Using the Wiser Home app, you can lock the thermostat controls (nothing will happen when the thermostat rotary push-button is turned clockwise or anti-clockwise). This will prevent children from changing the temperatures in your room by playing with it.
  1. On the Home screen, tap .
  2. Tap Devices > > Device Lock (A) to lock or unlock the thermostat control.
    TIP: When the thermostat lock is active, a will appear next to the thermostat.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.