DUG_Connected Thermostat 16 A, ZB_WH-06

About the device

The Connected Thermostat Insert 16 A (hereinafter referred to as Thermostat) is mainly used for electric underfloor heating or electric radiators, but could also be used to control mains powered motorized valves or circulating pumps for water based heating.

The thermostat consists of:

  1. Connected Thermostat Insert 16 A (MEG5777-0001)

  2. Frame

  3. Connected Thermostat Module, ZB (MEG5779-0xxx, MEG5779-60xx)

NOTE:
  • The insert works with several floor sensor types. Refer floor sensor setting.

  • The room air temperature sensor is included with the Connected Thermostat Module, ZB.

The thermostat is composed of three components: inserts, frame, and ZB module, and each must be ordered separately.


Thermostat features:

  • Measure & control the room temperature

  • Dot-matrix displays (current room and set temperature)

  • Device lock

  • Valve Protection

  • Heating changeover

  • Universal input setback/presence (external)

  • Volt-free or live control, normally open or normally closed.

  • Smart schedule through a Wiser app

Operating elements

  1. Dot-matrix display

    • Wireless connectivity LED ()

    • Heating demand LED ()

    TIP: All LED indications are explained in the LED behavior chapter.
  2. Rotary push-button

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.